The S32K312 DMA + IDLE fails to receive data.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

The S32K312 DMA + IDLE fails to receive data.

499 Views
li3
Contributor II

Hi NXP,

S32K312 I use DMA to receive data and promise to receive data in Buffer in IDLE interrupt callback function. When the program runs and the first IDLE interrupt occurs, the receiving Buffer can receive data and print it, but the second time to send data, the receiving Buffer does not receive data.

If I don't print in IDLE interrupt callback receive the data in Buffeer. In Debug mode, you can see that data is normally received in the receiving Buffer.

Please help me solve this problem in conjunction with my project. thank you.

li3_0-1717079046244.png

li3_0-1717079676071.png

 

Best  Regards,
Li 3

0 Kudos
Reply
7 Replies

478 Views
li3
Contributor II

Why uint8_t uartrxBuffer[256]; Put it in ".mcal_bss_no_cacheable" and it'll work, okay? Please explain the reason. Thank you.

li3_0-1717134210334.png

 

0 Kudos
Reply

443 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @li3,

If the DMA writes to the buffer, you have no guarantee whether the data the core reads is from the buffer in sram or from the cache. The buffer must be either in a non-cacheable sram, or you would need to invalidate the cache each time before the core reads it.

 

Regards,

Daniel

0 Kudos
Reply

440 Views
li3
Contributor II

Hi Daniel,

Thanks for your reply, I understand what you mean. If RXbuffer is in non-cacheable sram, the cache should be invalidated before each read, if not, it will only affect the read operation.

But after I read the RXbuffer, why can't I write data to the RXbuffer using DMA? I don't understand the connection. Please elaborate. Thank you.

 

Best  Regards,
Li 3

0 Kudos
Reply

422 Views
danielmartynek
NXP TechSupport
NXP TechSupport

The DMA can write to the buffer, but the core does not see the data in the buffer written by the DMA, because it reads the cache instead.

 

BR, Daniel

0 Kudos
Reply

393 Views
li3
Contributor II

Hi Daniel,

The rxbuffer I write is a receive array that I define. I used debug mode to view the data stored in the rxbuffer and found that after printing the data in the rxbuffer, DMA cannot receive the data sent by the PC, while rxbuffer still has the previous data. Why is this?

Combined with my above project, answer it, thank you.

li3_0-1717464755233.png

 

 

Best  Regards,
Li 3

0 Kudos
Reply

361 Views
danielmartynek
NXP TechSupport
NXP TechSupport

HI @li3,

If I'm not mistaken, you have already confirmed that it works when the buffer is in a non-cacheable memory.

This is the expected behavior of the cache.

 

Regards,

Daniel

0 Kudos
Reply

357 Views
li3
Contributor II

Hi Daniel,

Yes, this receive array goes into non-cacheable memory and receives fine.

I want to know that I put the receive array into the cacheable memory, do a print or copy of the data in the receive array, and find that DMA can not receive data.

But do not print or copy the receiving array, DMA can normally receive data, why?

 

Regards,

Li 3

0 Kudos
Reply