The CAN transfer bitrate configured on the S32DS is different from that detected by the CAN tool

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

The CAN transfer bitrate configured on the S32DS is different from that detected by the CAN tool

ソリューションへジャンプ
832件の閲覧回数
shuo41
Contributor III

The CAN transfer bitrate configured on the S32DS is different from that detected by the CAN tool,why?bitrate configured by s32dsbitrate configured by s32dscan tool on pc(through can Analyser)can tool on pc(through can Analyser)

0 件の賞賛
返信
1 解決策
694件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

share project which shows the issue so we can check.

BR, Petr

 

元の投稿で解決策を見る

0 件の賞賛
返信
7 返答(返信)
816件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

check if selected protocol clock is really the one you specified (40MHz) within clock config.

BR, Petr

0 件の賞賛
返信
805件の閲覧回数
shuo41
Contributor III

It is 40MHZ 

clock.pngclock2.png

0 件の賞賛
返信
796件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

then check if clock is really configured and system clock running from PLL. Also measure TXD line with scope/analyzer to know real bitrate.

You can also check FlexCAN bit timing registers for values written.

BR, Petr

 

0 件の賞賛
返信
699件の閲覧回数
shuo41
Contributor III

I am testing LIN.When I fill in the baud rate column with 9600, my logic analyzer cannot receive data correctly at 9600.When I fill in the baud rate column with 3700, my logic analyzer correctly receives data at 9600.22.png44.png77.png66.png55.png

0 件の賞賛
返信
695件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

share project which shows the issue so we can check.

BR, Petr

 

0 件の賞賛
返信
675件の閲覧回数
shuo41
Contributor III

HI,I Solved the problem. My external clock configuration is incorrect.The external clock is 40MHz, and I have configured it to be 16MHz.Thinks for your help.

0 件の賞賛
返信
701件の閲覧回数
shuo41
Contributor III

Its source is PLL, that's right. The bit rate measured by my oscilloscope is incorrect.I test Lin, The baud rate it outputs is also incorrect.11.png

0 件の賞賛
返信