Temperature detection function

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Temperature detection function

564 次查看
JackChen2022
Contributor I

Hello, I would like to know if the S32K14* series chips have a temperature detection function, or if the entire S32K series has this function, you can also provide reference.

0 项奖励
回复
3 回复数

557 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi JackChen2022,

Please refer to: https://community.nxp.com/t5/S32K/S32K148-ADC-Temp-Sense/m-p/1071115

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复

555 次查看
JackChen2022
Contributor I

Hi Robin_Shen ,After reading your reply, I understand that the function of the internal temperature sensor may be supported on earlier hardware, and the existing version may be removed? At the same time, some sample programs are not available yet, right?

0 项奖励
回复

550 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

the existing version may be removed? no

some sample programs are not available yet, right? still not sample programs.

0 项奖励
回复