TJA1153 PINOUT & Datasheet

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

TJA1153 PINOUT & Datasheet

跳至解决方案
647 次查看
KarthikRaja
Contributor I

Hi,

For a product development, we are planning to use S32K MCU along with Secure CAN chip TJA1153. Could you provide technical datasheet as I could not find in online. I need to know the PINOUT, voltage levels, operating modes and other features.

 

Thanks

Karthik Raja

0 项奖励
回复
1 解答
620 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Karthik,

The TJA1153A datasheet as well as other useful documentation are classified as Secure Files requiring an NDA.

If your company has not signed the NDA with NXP yet, you can request it from:
https://www.nxp.com/support/support:SUPPORTHOME

If there is a valid NDA in place, you can download the datasheet from:
https://www.nxp.com/products/interfaces/can-transceivers/secure-can-transceivers/secure-hs-can-trans...

Capture 2.JPG

Please make sure you are signed in to nxp.com. If you do not see the datasheet, please click on "Request additional access" or edit your secure access rights by going to My NXP > Profile. For more information about secure access rights, please refer to this website:
https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS


The TJA1153A is a standalone HS-CAN transceiver with Sleep mode offering these security features:

Capture 3.JPG

In case there are no security violations detected, the TJA1153A behaves like a standard HS-CAN transceiver such as the TJA1443ATK.

BR, Tomas

在原帖中查看解决方案

0 项奖励
回复
4 回复数
621 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Karthik,

The TJA1153A datasheet as well as other useful documentation are classified as Secure Files requiring an NDA.

If your company has not signed the NDA with NXP yet, you can request it from:
https://www.nxp.com/support/support:SUPPORTHOME

If there is a valid NDA in place, you can download the datasheet from:
https://www.nxp.com/products/interfaces/can-transceivers/secure-can-transceivers/secure-hs-can-trans...

Capture 2.JPG

Please make sure you are signed in to nxp.com. If you do not see the datasheet, please click on "Request additional access" or edit your secure access rights by going to My NXP > Profile. For more information about secure access rights, please refer to this website:
https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS


The TJA1153A is a standalone HS-CAN transceiver with Sleep mode offering these security features:

Capture 3.JPG

In case there are no security violations detected, the TJA1153A behaves like a standard HS-CAN transceiver such as the TJA1443ATK.

BR, Tomas

0 项奖励
回复
560 次查看
KarthikRaja
Contributor I

Hi

 

Thanks for that information.


When I checked Evaluation boards BOM, S32K3X4EVB is using TJA1443ATK but in the interface list & in the block diagram it is shown as TJA1153. 

Are both same or why it is still given like this. Kindly clarify which CAN transceiver is used in S32K3X4EVB board.

 

 

 

 

0 项奖励
回复
643 次查看
KarthikRaja
Contributor I
Hi
When I checked Evaluation boards BOM, S32K312EVB is using TJA1043TKY part and S32K3X4EVB is using TJA1443ATK but in the interface list it is shown as TJA1153 is used in S32K3X4EVB.

Can you please clarify this.
0 项奖励
回复
642 次查看
KarthikRaja
Contributor I

Hi,

And also when I checked S32K3X4EVB interfaces it is given as TJA1153 is used but when I checked BOM I found TJA1443ATK chip is used. But I see TJA1443 chip is not secure CAN. 

 

Can you clarify this, or secure CAN is something to do with algorithms?

0 项奖励
回复