[Support] How to rom writing FS32K148 by Behive204 machine?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[Support] How to rom writing FS32K148 by Behive204 machine?

1,077 Views
BradNguyen
Contributor I

Hello,

I am using Behive 204 programer machine to Rom writing FS32K148 and try to find correct way to do it.

While do setting step, there are some option need to choose (FlexNVM partition/FLASH/DFLASH/EEPROM) but i dont know which option is correct to choose. 

(please refer the picture)

Please help me about this case.

0 Kudos
Reply
3 Replies

1,048 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @BradNguyen 

The S32K148 It is programmed by FLASH and according to the information you provide, you are doing it right, I suggest you contact Elnec support through the following link: Technical support | Elnec 

 

B.R.

VaneB

0 Kudos
Reply

1,069 Views
BradNguyen
Contributor I

Dear bros,

I try to tick on Flash in the 1st time  and Flash/DFlash in the 2nd time but software is not wrote into the FS32K IC after mount into PCBA. I think there was something wrong at setting at behive 204 machine but i could not find out correct way. please help with thanks

0 Kudos
Reply

1,076 Views
BradNguyen
Contributor I

Hi,

I attach the picture of setting

0 Kudos
Reply