Should I get a PEmicro Cyclone or Segger Jlink?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Should I get a PEmicro Cyclone or Segger Jlink?

1,525件の閲覧回数
rvalente
Contributor III

Hello mates, I'm just getting started on a project with the S32K, so far, great uC.

Target is the S32K118, i;m not sure if I should get the pemicro or the segger J-link...

PEMicro pros:
Live view on S32DS (can't believe segger wont work)


Segger pro:
Student Version with most of the resources available (but probably will get a jlink base)
Cross use with many vendors (e.g: ST and Renesas)
Bigger community
A lot of tools from segger (like JScope)


0 件の賞賛
3 返答(返信)

1,497件の閲覧回数
rvalente
Contributor III

Hello Mr Jiri,

do you know any limitation of the Jlink edu vs the base for the S32K?

0 件の賞賛

1,482件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

the only Segger limitation what I remember is, that Segger j-link performs device reset when you are attaching to running target.

I'm not familiar with the student version - Segger probably have described differences between educational and full version on their web page. 

 

Jiri

0 件の賞賛

1,500件の閲覧回数
jiri_kral
NXP Employee
NXP Employee

Hi, 

unfortunately Segger under S32DS doesn't have such view (realtime view). But you can use external segger's tools - as you mentioned - for example j-scope, which can be run in parallel with your debug session.  So, from my point of view - Segger is winner! 

 

Hope it helps. 

Jiri