SWD pins and reset_b pins of S32K146 are configured as normal IO.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SWD pins and reset_b pins of S32K146 are configured as normal IO.

Jump to solution
653 Views
ananan
Contributor III

SWD pins and reset_b pins of S32K146 are configured as normal IO. How do I recover it?

0 Kudos
1 Solution
642 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ananan,

Seems that you already refer to the discussion in https://community.nxp.com/t5/S32K/Open-SDA-P-amp-E-Error/td-p/1497523

Did you download the Kinetis_Recovery_Utility.zip from there? PEMicro USB Multilink Universal Rev C should able to use to test. But please update it's firmware first.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
5 Replies
650 Views
ananan
Contributor III

ananan_0-1683608620517.png

 

0 Kudos
643 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi ananan,

Seems that you already refer to the discussion in https://community.nxp.com/t5/S32K/Open-SDA-P-amp-E-Error/td-p/1497523

Did you download the Kinetis_Recovery_Utility.zip from there? PEMicro USB Multilink Universal Rev C should able to use to test. But please update it's firmware first.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
626 Views
ananan
Contributor III

I solve the problem when I connect the TVCC pin,thank you very much!

628 Views
ananan
Contributor III

I usethe three pins, DIO pin, CLK pin,GND pin。

0 Kudos
635 Views
ananan
Contributor III
 
 
 

微信图片_20230509185754.png

I power board by hands cycling,but it does   not operation successfully

0 Kudos