SRAMU contents are retained across resets

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRAMU contents are retained across resets

442 Views
TM_207
Contributor I

Hello

When I was working on the S32K144-BootLoader, I was driven by this requirement:

I use the UDS protocol, when the  APP receives a programming command from the diagnostics, the APP performs a soft reset and marks (BootJumpFlag = 1), Because the soft reset program starts from the beginning, the program enters the boot . the boot program detects the BootJumpflag == 1 , stay in the Boot program all the time, do not jump. Please what can I do to ensure that the BootJumpFlag does not return to zero after a soft reset.

The reference manual says register CHIPCTL  SRAMU_RETE=0, SRAM_U is saved after a soft reset, SRAMU_RETE the default value is 1. How can I do this SRAMU_RETE this bit to keep the current value after a soft reset.

0 Kudos
Reply
1 Reply

415 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@TM_207

you can refer to S32K-RM rev13,the chapter :31.3.4 SRAM retention:power modes and resets

The SRAM data will not be lost during the software reset proces,nut will be lost during the power-down reset.The purpose of this register is to ensure that the data in the RAM cannot be accessed during the software reset process.

I suggest you use Flash area to store these flags.

0 Kudos
Reply