Hello,
im using the TL9261 as SBC and is controlled from S32K148 by the following config :
i search in the SDK for the corresponding lib to generate the driver for me, but its not there, so i found this repo in github. it has the functions i need like (read register field,write register...)
its now integrated in my project but i dont know how to initialise the SBC, since the implementation of 'SBC_SPI_INIT' is not compatible with my controller.
i attached the source code.
Best regards.
Solved! Go to Solution.
Hi Badre,
SDK supports FS45xx, UJA116x and UJA113x SBC devices from NXP. If you want to use other SBC, it's necessary to develop own driver. This is up to user.
Regards,
Lukas
Hi Badre,
SDK supports FS45xx, UJA116x and UJA113x SBC devices from NXP. If you want to use other SBC, it's necessary to develop own driver. This is up to user.
Regards,
Lukas