S32K34x Low power mode result

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K34x Low power mode result

跳至解决方案
845 次查看
OliverTian
NXP Employee
NXP Employee

Hello, 
    Based on the minimum system board (all IOs are floating) of S32K34x, the low power mode result is as Datasheet.
    Hope will be helpful for you as reference. 

OliverTian_0-1689053536546.png
Cheers !
Oliver

 



0 项奖励
回复
1 解答
844 次查看
OliverTian
NXP Employee
NXP Employee

S32K3 mini EVB:

* Support both S32K344 and S32K312 (HDQFP172);
* All GPIO extended out;
* 1 User LED (can be routed to any pin), 1 reset LED, 1 power LED;
* 1 User switch (can be routed to any pin), 1 reset switch;
* Can be programmed by 10 pin JTAG debug port or 5pin SWD debug header;
* Power the MCU by type C(5V) cable or Header H1 (VDD_HV_A and B have to be the same voltage);
* I2C pull up resisters(Can be routed to any I2C pin);
* 16MHZ crystal;
* Size: 9x7cm;

在原帖中查看解决方案

0 项奖励
回复
1 回复
845 次查看
OliverTian
NXP Employee
NXP Employee

S32K3 mini EVB:

* Support both S32K344 and S32K312 (HDQFP172);
* All GPIO extended out;
* 1 User LED (can be routed to any pin), 1 reset LED, 1 power LED;
* 1 User switch (can be routed to any pin), 1 reset switch;
* Can be programmed by 10 pin JTAG debug port or 5pin SWD debug header;
* Power the MCU by type C(5V) cable or Header H1 (VDD_HV_A and B have to be the same voltage);
* I2C pull up resisters(Can be routed to any I2C pin);
* 16MHZ crystal;
* Size: 9x7cm;

0 项奖励
回复