S32K344 flash

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,801件の閲覧回数
Neo1096
Contributor III

hello, I have several questions about S32K344 flash:

1.pflash erases only 1000 times? Isn't the erasure of flash used to store code around 10,000 times in general?

2.Is the minimum programming unit of flash 1bit or 8bit or 32bit or 64bit? I can't find it in the datasheet. What exactly is the alignment of the other bytes? For example, if I write an 8bit and then write a 16bit, can I also write a 32bit in this 64bit storage area? Is the alignment of dflash and pflash the same?

3.Is it possible to provide a demo about RTD-based dflash simulate eeprom? If not, can you provide a FEE code idea or documentation?

4.I want to achieve power down save function, save 1KB of data to dflash, MCU power supply is 5V, circuit board input power is 48V, how much power down hold capacitor do I use?

thank you.

 

 

 

 

0 件の賞賛
返信
1 解決策
2,763件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Neo1096 

1. You can find the specification in the datasheet:
https://www.nxp.com/docs/en/data-sheet/S32K3xx.pdf

lukaszadrapa_0-1709555241472.png

 

2. This can be found in the reference manual:

lukaszadrapa_1-1709555252885.png

3. You can find the demo in RTD in FEE folder:
c:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\Fee_TS_T40D34M40I0R0\examples\S32DS\S32K3XX\Fee_Example_S32K344\

4. This is application dependent, we do not have recommendation for this.

Regards,
Lukas

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,764件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @Neo1096 

1. You can find the specification in the datasheet:
https://www.nxp.com/docs/en/data-sheet/S32K3xx.pdf

lukaszadrapa_0-1709555241472.png

 

2. This can be found in the reference manual:

lukaszadrapa_1-1709555252885.png

3. You can find the demo in RTD in FEE folder:
c:\NXP\S32DS.3.5\S32DS\software\PlatformSDK_S32K3\RTD\Fee_TS_T40D34M40I0R0\examples\S32DS\S32K3XX\Fee_Example_S32K344\

4. This is application dependent, we do not have recommendation for this.

Regards,
Lukas

0 件の賞賛
返信