S32K344 eval-board flash application bin file via CAN UDS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

S32K344 eval-board flash application bin file via CAN UDS

110 次查看
Dan_L
Contributor I

We are following the steps defined in ECUBUS_344CAN_uds.json of the unified_bootloader_demo_V2.1 package to flash S32K344_CAN_App_RTD200 images onto to S32K344 eval board. Both .bin and .elf images can be flashed successfully via the UDS-TP stack. However, only the elf image can operate normally. The bin image always crashes when calling Boot_JumpToApp. Is there something extra need to do when flashing the S32K344_CAN_App_RTD200.bin image? This bin image has been verified with J-Link which can operate normally.

 

0 项奖励
0 回复数