S32K344 - What is the max BCTU list items ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K344 - What is the max BCTU list items ?

Jump to solution
491 Views
kyf
Contributor V

Hello NXP team !

 

Hello there, I've tried to create a BCTU list with 36 items. But when I'm trying to do so I get the error message bellow at the "peripheral tool":

Issue: There are too many channels in the command list array.
Level: Error
Type: Tool problem
Tool: Peripherals
Origin: Peripherals:BOARD_InitPeripherals
Resource: Bctu_Ip
Information: There are too many channels in the command list array.

What can I do to work around this ? I've never thought that there would be a limit to the BCTU list items.

The setup that I'm trying to do here is to have 3x 12 ADC conversions and then start all over again. I'm also utilizing FIFO1 + watermark lvl to achieve 36 ADC conversions (18 parallel ones ADC0/1).

 

Kind regards,

kyf

0 Kudos
1 Solution
482 Views
kyf
Contributor V

I've been given the chance to answer my own post !!

kyf_6-1679914181499.png

 

 

View solution in original post

0 Kudos
2 Replies
483 Views
kyf
Contributor V

I've been given the chance to answer my own post !!

kyf_6-1679914181499.png

 

 

0 Kudos
484 Views
kyf
Contributor V

Here are some screenshots:

kyf_0-1679912837881.pngkyf_2-1679912920165.png

 

Is the max size of BCTU list 255 ?

 

kyf_4-1679913021468.png

kyf_5-1679913367388.png

 

 

 

 

 

 

0 Kudos