I use s32k344, RTD 1.0.0
I want to implement three arrays into three sending mailboxes at a timer interval of 1s, polling in the main function, handling in the interrupt. But how do I know if I didn't send or receive it in loop mode? At present, I can only receive the first set of three data, and the following two data cannot be received. Is there any flag that needs to be cleared?
#S32K344
Solved! Go to Solution.
Hi,
after successful receive you need to call Receive function again, to update internal driver structure and enable MB interrupt again, if used.
BR, Petr
got it
Hi,
after successful receive you need to call Receive function again, to update internal driver structure and enable MB interrupt again, if used.
BR, Petr