S32K314 Flex IO i2S and SAI port

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K314 Flex IO i2S and SAI port

964 Views
Pravinkumar
Contributor I

Hi,

I would like to know the advantages/disadvantages of Flex IO I2S over SAI. And, why you someone use FlexIO i2S when the same functionality can be achieved with SAI ?

0 Kudos
Reply
5 Replies

956 Views
Pravinkumar
Contributor I

But, will we have any system related issues when FLEXIO is selected over SAI ?

 

Thank you

Pravinkumar

0 Kudos
Reply

946 Views
danielmartynek
NXP TechSupport
NXP TechSupport

The SAI module has much more HW features than the FlexIO.

There are TX/RX FIFOs, Sync and FIFO error flags / warnings / interrupts, etc.

You can compare the two modules in these application notes:

 

AN12202 Using Synchronous Audio Interface (SAI) on S32K148

https://www.nxp.com/docs/en/application-note/AN12202.pdf

AN12174 Using FlexIO to emulate communications and timing peripherals

https://www.nxp.com/docs/en/application-note/AN12174.pdf

 

Regards,

Daniel

 

0 Kudos
Reply

937 Views
Pravinkumar
Contributor I

Thank you.

 

I also would like to understand interrupt load in both cases, is it same or different, is there any document explaining the same ?

 

The reason I am asking is that we created a design using Flex IO and but I would like to know if there would be any implications of not using SAI.

0 Kudos
Reply

926 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @Pravinkumar,

There is no such document.

I should mention that the RTD versions have Quality packages.

For example: SW32K3_RTD_4.4_2.0.2_D2211_QualityPackage.zip

 

But the interrupt load and other implication are also application dependent.

The modules are different, the drivers are different.

You can compare, for example, the callback event types of the two drivers:

Flexio_I2s_Ip_Types.h

danielmartynek_1-1681983884304.png

Sai_Ip_Types.h

danielmartynek_0-1681983843006.png

 

Regards,

Daniel

 

 

 

0 Kudos
Reply

957 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @Pravinkumar,

The SAI is a dedicated module for I2S and other protocols.

Whereas the FlexIO just emulates the protocols.

FlexIO is used when there is no SAI module on the part, or if more channels are needed.

 

Regards,

Daniel

 

0 Kudos
Reply