S32K312 Standby Current Consumption about CAN

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K312 Standby Current Consumption about CAN

Jump to solution
1,001 Views
kjy106906
Contributor IV

Hello @danielmartynek 

Thanks for your help.

https://community.nxp.com/t5/S32K/S32K312-Standby-Current-Consumption/m-p/1503807/highlight/false#M1...

I have more questions.

kjy106906_0-1660731049004.png

 

Here, I additionally set CAN and entered Standby, and the current consumption is high.(about 300uA)

(Low current consumption (about 50uA) when there is only GPIO)

please tell me the cause.

Best Regards

 

0 Kudos
1 Solution
986 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

If the port is routed to the FlexCAN modele, it cannot be controlled like GPIO.

This is really application-dependant, but if you see higher power consumption, you can reconfigure it to GPIO and set it as needed to eliminate any additional current there.

 

BR, Daniel

View solution in original post

0 Kudos
7 Replies
996 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello @kjy106906,

In general, input pins should be driven or pulled to either VSS or VDD to avoid leakage current on that pins.

Outputs should not drive any external load.

Not sure what is the state of the pins in the low power mode of your application, I haven't seen the schematic.

 

BR, Daniel

 

 

0 Kudos
990 Views
kjy106906
Contributor IV

Thank you @danielmartynek 

The moment CAN TX is port inited, the pin is set to High.
Is there a way to set this to Low when going to Standby?

Best Regards

0 Kudos
987 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

If the port is routed to the FlexCAN modele, it cannot be controlled like GPIO.

This is really application-dependant, but if you see higher power consumption, you can reconfigure it to GPIO and set it as needed to eliminate any additional current there.

 

BR, Daniel

0 Kudos
969 Views
kjy106906
Contributor IV

Thank you @danielmartynek 

The S32K1XX SDK shows the appropriate function.
PINS_DRV_SetMuxModeSel
But I can't find a suitable function in the S32K3XX RTD.
Can you recommend a suitable function for the S32K3XX RTD?

Best Regards

0 Kudos
967 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi @kjy106906,

Have a look at Siul2_Port_Ip.c

Siul2_Port_Ip_SetOutputBuffer()

Siul2_Port_Ip_SetInputBuffer()

 

BR, Daniel

 

 

0 Kudos
963 Views
kjy106906
Contributor IV

Thank you @danielmartynek 

The pin configuration has various parameters.
Is there any problem if I just call that function?

Siul2_Port_Ip_SetOutputBuffer

kjy106906_0-1661245654992.png

I am concerned about the differences as follows.

kjy106906_1-1661245729361.png

Best Regards

0 Kudos
960 Views
danielmartynek
NXP TechSupport
NXP TechSupport

From the S32K3xx RM:

danielmartynek_0-1661246322694.png

So, you need to disable the input buffer provided it is enabled.

 

BR, Daniel

 

0 Kudos