Hi, I want to store and use the interrupt vector in SRAM (0x20400000) however I dont get any interrupts when I have the interrupt vector stored there. But if I change it to be stored in DTCM it works.
I don't use MPU nor enable I & D-cache. Could this be the issue? Whats the work around?
After some investigation over the weekend, it seems that it is the stack that doesnt work properly for me. Earlier I had the stack in DTCM, but due to limit space I want to either move the stack to SRAM or ITCM.
It is usual to have stack located is SRAM, DTCM may be suitable option as well, ITCM only with using of backdoor access.
I would recommend to use some S323DS example project as a startup. You could possible share details about your configuration.
I'm using example code as reference and I can see that some examples dont even use DTCM nor ITCM and only SRAM.
The latest status is that it works when I flash the application and run the code, but when I power off and power on the MCU it doesnt work anymore in SRAM.
However, it works after power toggle if I have MPU enabled. Can it be that SRAM have a certain configuration without MPU that interfere?