Hello
When I use DS3.5 to generate C40 code to operate Flash, I found that there is only an interface for erasing Sector (C40_Ip_MainInterfaceSectorErase) in C40Ip.c, but I checked RM and found that bit[ESS] of register MCR can be set to erase Block of. Is there an interface to erase the Block?
BestRegards
Simon
已解决! 转到解答。
In the RM 21.7.1.2, you may read statement that:
„Block erase is for Factory use only, under controlled conditions.“
The Program/Erase cycles value is specified as 25, when using the Block Erase. That’s why flash drivers and external tools do not use this operation.
In the RM 21.7.1.2, you may read statement that:
„Block erase is for Factory use only, under controlled conditions.“
The Program/Erase cycles value is specified as 25, when using the Block Erase. That’s why flash drivers and external tools do not use this operation.
Thank you for your answer.
I saw this description in RM before, I thought that there was a way to enter the factory mode, now I understand that the block cannot be erased by the driver.
BestRegards
Simon