S32K3 Number of SWT instances.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K3 Number of SWT instances.

586 Views
li3
Contributor II

Hi NXP,

Why is it found in Section 67 that S32K328, 338, 348, 358 support 3 SWT instances? We do see in section 2.5 that 2, 3, 1, and 2 SWT instances are supported respectively.

li3_0-1712887371101.pngli3_1-1712887530832.png

Best regards,

Li 3.

 

0 Kudos
Reply
5 Replies

563 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

SWT chapeter description does not look correct to me.

You have one SWT for one active core (not for lockstepped), so you can refer to this simple rule.

petervlna_0-1712904084932.png

Table 5. is correct.

Best regards,

Peter

 

0 Kudos
Reply

561 Views
li3
Contributor II

Hi HXP,

Is CM7_0-CM7_1 a kernel? Does Disable mean an unwanted kernel?

li3_0-1712905775427.png

Best regards,

Li 3.

0 Kudos
Reply

557 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Disabled in this case means N/A. There is no point to have that column in the manual as those cores are not available.

Best regards,

Peter

0 Kudos
Reply

543 Views
li3
Contributor II

Hi HXP,

Is CM7_0-CM7_1 a kernel?

What is Lockstep and Decoupled?

li3_0-1712995307288.png

 

Best regards,

Li 3.

0 Kudos
Reply

484 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

From general uC theory:

Dual-redundant core (lock-step) CPU functionality

One of the most common techniques for implementing replication in automotive MCUs is called 'lockstep'. Lockstep means that two processors are running the same set of operations in parallel. The two sets of results are compared by a checker unit or comparator to look for single point faults.

 

Decoupled

Independent operation on each core.

Best regards,

Peter

0 Kudos
Reply