Hi
I am using S32K148 and got a problem with lpuart1 receving.
I use ProcessorExpert to generate code. Below is the UART setting
Transfer type: interrupt
Parity mode: disable
Stop bits: 1
Bits per char: 8
My below function keeps reading continuous bytes in a if statement in main thread.
LPUART_DRV_ReceiveData(INST_LPUART1,&Buffer[BufferCount],1);
The below isr indicates received data for the main thread, and increments the BufferCount.
void rxcallback(void *driverState, uart_event_t event, void *userData)
{
/* Unused parameters */
(void)driverState;
(void)userData;
/* Check the event type */
if (event == UART_EVENT_RX_FULL)
{
uart_flag = 1 // used for indication of rx received
BufferCount++;
}
}
When the LPUART_DRV_IRQHandler is called, it's occationally stuck in the line below for around 1 ms(in the function: LPUART_SetReceiverCmd(base, false);), which causes lost to a byte . (it usually takes 3us for the function: LPUART_SetReceiverCmd(base, false);)
while((bool)((base->CTRL & LPUART_CTRL_RE_MASK) != 0U) != enable) {}
When I comment out the line in lpuart_hw_access.h, the UART works just fine. UART can keep continuous reading steadily. What could be the cause for the mask operation to take this long?
static inline void LPUART_SetReceiverCmd(LPUART_Type * base, bool enable)
{
base->CTRL = (base->CTRL & ~LPUART_CTRL_RE_MASK) | ((enable ? 1UL : 0UL) << LPUART_CTRL_RE_SHIFT);
/* Wait for the register write operation to complete */
// while((bool)((base->CTRL & LPUART_CTRL_RE_MASK) != 0U) != enable) {}
}
an I found a similar problem in here: S32K146 LPUART EDMA failed - NXP Community
The difference is the transfer type only I guess
Best Regards,
Joe
解決済! 解決策の投稿を見る。
Hi @JOE_1209,
This can happen when the receiver is already receiving a new character.
Can you tried with a lower baudrate?
Or can you increase the system clock frequency?
The SDK drivers have rather significant CPU load.
Regards,
Daniel
Hi @JOE_1209,
This can happen when the receiver is already receiving a new character.
Can you tried with a lower baudrate?
Or can you increase the system clock frequency?
The SDK drivers have rather significant CPU load.
Regards,
Daniel
Hi Daniel,
Thanks for the reply.
It has been fixed by putting LPUART_DRV_SetRxBuffer in the interrupt for UART receive. No need to change the frequency.
Regards,
Joe