[S32K146] : FTM pwm activation not working

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[S32K146] : FTM pwm activation not working

1,333 Views
sebastien_ledio
Contributor I

Hello,

I would like to manage 2 PWMs (on pin PTC15 (FTM1_CH3, ALT2) & PTD8(FTM1_CH4, ALT6)), and just after starting counter, the signals (on pin) rise, but stay in high level (3,3v), so I have not PWM.

My source code comes from NXP example, but I show you it:

  /* FTM1 Clocking */
  PCC->PCCn[PCC_FTM1_INDEX] &= ~PCC_PCCn_CGC_MASK;  /* Ensure clk disabled for config  */
  PCC->PCCn[PCC_FTM1_INDEX] |= PCC_PCCn_PCS(2)      /* Clock Src=1, 8 MHz SIRCDIV1_CLK */
                            |  PCC_PCCn_CGC_MASK;   /* Enable clock for FTM regs       */

  /* FTM1 Initialization */
  FTM1->MODE |= FTM_MODE_WPDIS_MASK;  /* Write protect to registers disabled (default)             */
  FTM1->SC    = FTM_SC_PWMEN3_MASK    /* Enable PWM channel 3 output                               */
               |FTM_SC_PWMEN4_MASK    /* Enable PWM channel 4 output                               */
               |FTM_SC_PS(3);         /* TOIE (Timer Overflow Interrupt Ena) = 0 (default)         */
                                      /* CPWMS (Center aligned PWM Select) = 0 (default, up count) */
                                      /* CLKS (Clock source) = 0 (default, no clock; FTM disabled) */
                                      /* PS (Prescaler factor) = 7. Prescaler = 128                */

  FTM1->CONF |= FTM_CONF_BDMMODE(3);  /* FTM functionnal mode debug */

  FTM1->COMBINE = 0x00000000;  /* FTM mode settings used: DECAPENx, MCOMBINEx, COMBINEx=0 */
  FTM1->POL = 0x00000000;      /* Polarity for all channels is active high (default)      */
  FTM1->MOD = 62500 -1 ;       /* FTM1 counter final value (used for PWM mode)            */
                               /* FTM1 Period = MOD-CNTIN+0x0001 ~= 62500 ctr clks        */
                               /* 8MHz /128 = 62.5kHz ->  ticks -> 1Hz                    */

  /* FTM1, Channel 3 in PWM Mode */
  FTM1->CONTROLS[3].CnSC = FTM_CnSC_MSB_MASK
                          |FTM_CnSC_ELSB_MASK;  /* FTM1 ch3: edge-aligned PWM, low true pulses       */
                                                /* CHIE (Chan Interrupt Ena) = 0 (default)           */
                                                /* MSB:MSA (chan Mode Select)=0b10, Edge Align PWM   */
                                                /* ELSB:ELSA (chan Edge/Level Select)=0b10, low true */
  /* FTM1, Channel 4 in PWM Mode */
  FTM1->CONTROLS[4].CnSC = FTM_CnSC_MSB_MASK
                          |FTM_CnSC_ELSB_MASK;  /* FTM1 ch4: edge-aligned PWM, low true pulses       */
                                                /* CHIE (Chan Interrupt Ena) = 0 (default)           */
                                                /* MSB:MSA (chan Mode Select)=0b10, Edge Align PWM   */
                                                /* ELSB:ELSA (chan Edge/Level Select)=0b10, low true */
  FTM1->CONTROLS[3].CnV =  46875;    /* FTM1 ch3 compare value (~75% duty cycle) */
  FTM1->CONTROLS[4].CnV =  46875;    /* FTM1 ch4 compare value (~75% duty cycle) */

 /* Pins definitions
   * ==============================
   *
   * Pin number        | Function
   * ----------------- |-----------
   * PTC15             | FTM1CH3
   * PTD8              | FTM1CH4    */

  PCC->PCCn[PCC_PORTC_INDEX ]|=PCC_PCCn_CGC_MASK;   /* Enable clock for PORTC */
  PCC->PCCn[PCC_PORTD_INDEX ]|=PCC_PCCn_CGC_MASK;   /* Enable clock for PORTD */
  PORTC->PCR[15]|=PORT_PCR_MUX(2);                  /* Port C15: MUX = ALT2, FTM1CH3 */
  PORTD->PCR[8]|=PORT_PCR_MUX(6);                   /* Port D8 : MUX = ALT6, FTM1CH4 */

  /* Start FTM1 counter with clk source = external clock (SOSCDIV1_CLK)*/

 FTM1->SC |= FTM_SC_CLKS(3);

Thanks by advance

Sebastien

0 Kudos
3 Replies

1,050 Views
sebastien_ledio
Contributor I

Hi,

response for Razvan-nicolae, I use example from NXP, but I used only the part code for PWM management, and my issue is fixed with the response ofDaniel (big thanks Daniel), but this code is done in the clock management, and I do not use this part of code  :smileyhappy:

Thanks for your answers.

0 Kudos

1,050 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

You need to enable the SIRCDIV1.

SCG->SIRCDIV = 0x00000001;

Regards,

Daniel

0 Kudos

1,050 Views
razva_tilimpea
NXP Employee
NXP Employee

Hi Sebastien,

Why you don't use SDK delivered with DesignStudio? There are some examples for PWM generation with FTM.

Best regards,

Razvan

0 Kudos