S32K144EVB can't enter debug, my co-workers modified the link files

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144EVB can't enter debug, my co-workers modified the link files

2,060 Views
hongjianzhang
Contributor III

The first question:  Today, after my co-workers modified the link files to change the ram mapping address in an project , he couldn't enter the debug session, and then mine project neither,  the computer could detect the open-sda port , and I had tried to upgrade the open-sda firmware app, but it  couldn't help.

Is the chip be secured or the opensda wrong,  I coultn't figure out what my co-workers done with the link files for now;

The second question , we found that the board couldn't plug out once we plug into our computer other than restart it, if not, we couldn['t get into the debug session;

Labels (1)
0 Kudos
Reply
8 Replies

1,750 Views
raresvasile
NXP Employee
NXP Employee

Hi,

What modifications were made to the linker file?

Did you modify flash_config or m_interrupts sections?

Best regards,

Rares

0 Kudos
Reply

1,750 Views
hongjianzhang
Contributor III

I think the chip is secured, but now I can't unsecured with opensda or jlink

Is that anything but replace a chip that i can do? 

0 Kudos
Reply

1,750 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

The FSEC register is loaded from 0x40C during the reset sequence, so it depends on what is the content of the byte in flash. If FSEC[SEC] != 0b10 and FSEC[MEEM] == 0b10, the MCU can't be unsecured (36.4.4.1.4 Flash Security Register (FSEC)).

Regards,

Daniel

0 Kudos
Reply

1,750 Views
hongjianzhang
Contributor III

the byte of 0x40C is 0x51, that is  FSEC[SEC] = 0b01, FSEC[MEEN] = 0b01, but I can't confirm it is the same with yesterday;

This chip may can't unsecure forever ?

0 Kudos
Reply

1,750 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hi,

if so the S32DS should be able to mass erase the MCU. 

What message do you get from the IDE? It should report that the MCU is secured and ask if you want to mass erase the device. 

Regards,

Daniel

0 Kudos
Reply

1,750 Views
hongjianzhang
Contributor III

The ide didn't report MCU is secured but reported can't get acess to the chip, I 'll paste the error tomorrow.

So we decided to repace the chip because we couldn't find a way to solve it

prayer_hong@163.com

0 Kudos
Reply

1,750 Views
hongjianzhang
Contributor III

in the s32k144_64_flash.ld:

m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000400
m_flash_config (RX) : ORIGIN = 0x00000400, LENGTH = 0x00000010
m_text (RX) : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0

modeified as below:

m_text1 (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000100
m_interrupts (RX) : ORIGIN = 0x00000100, LENGTH = 0x00000400
m_flash_config (RX) : ORIGIN = 0x00000500, LENGTH = 0x00000510
m_text2 (RX) : ORIGIN = 0x00000510, LENGTH = 0x0007FAF0

0 Kudos
Reply

1,750 Views
hongjianzhang
Contributor III

I can't figure out now, tomorrow i can try to understand what he did 

0 Kudos
Reply