Hello everyone.
Hope you're safe and sound.
My problem: after the code has been build and loaded on the target it works, but when I do a power cycle (power off, then on) the code doesn't start at all.
I did my development on a S32K142Q100 EVB and everything was fine.
Then I moved to my target PCBA which is with S32K144 (FS32K144ULT0VLLT). I think I've done all my settings correctly, considering the migration to the S32K144, incl. proper project settings (S32DS 2018.R1), replacing linker file (btw I use S32K144_64_flash.ld from the SDK).
My debugger is P&E micro Multilink universal, but I also tried it with Lauterbach's Trace32.
Can you suggest what miserable setting in the S32DS have I put wrong ...
I'll appreciate any help, and thanks for your time.
已解决! 转到解答。
Hello @munchosmith
The MCU must always do something.
If it does not keep resetting itself, the application is stuck somewhere.
You can attach the Multilink and examine the state of the MCU.
Regards,
Daniel
Hello @munchosmith
The MCU must always do something.
If it does not keep resetting itself, the application is stuck somewhere.
You can attach the Multilink and examine the state of the MCU.
Regards,
Daniel