S32K144-Q100 vs FRDMPK144-Q100

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144-Q100 vs FRDMPK144-Q100

1,674 Views
hjinha
Contributor II

I have two S32K144-Q100 & two FRDMPK144-Q100.

It is hard to find FRDMPK144-Q100. DataSheet. 

Can I flash download "S32K144-Q100" project  on FRDMPK144-Q100 without any Change ?

 

0 Kudos
Reply
3 Replies

1,543 Views
krisli
NXP Employee
NXP Employee

Hi,

This is not the right sub community for this question. You're talking about S32K, it's automotive ARM based 32-bit products. This sub-community is mainly for S08 products. www.nxp.com/s08

0 Kudos
Reply

1,543 Views
vicentegomez
NXP TechSupport
NXP TechSupport

I just move the thread to a better place.

0 Kudos
Reply

1,543 Views
danielmartynek
NXP TechSupport
NXP TechSupport

Hello, 

The FRDMPK144-Q100 board has a pre-production S32K144 maskset (0N77P).

There are many differences: different vector table, pinout, different number of peripheral instances...

Please use only the production version of S32K144 (0N57U).

Thanks, 

BR, Daniel

0 Kudos
Reply