Hi,
I want start the PDB with the Trigger_in0 Signal.
For the trigger_in0 signal I use the Compare Match trigger channel 0 from FTM0 with Trgmux.
TRGF(Bit7) from FTM0.EXTTRIG Register is set., but the PDB counter don't start.
How long must the trigger_in0 Signal pending, that the PDB counter start?
The FTM trigger channel 0 signal is only one clock cycle.
BR
Lutz
Hi,
The counter starts upon receiving a positive edge on the selected trigger input.
So, the problem must be in the PDB configuration.
Regards,
Daniel