S32K144, LPSPI SDI management

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144, LPSPI SDI management

Jump to solution
893 Views
Franky31
Contributor I

Hello,

I'm using SPI to dialog with an external chip (specific ADC). I'm using SDK functions.

At some point, to check if conversion is done, I have to keep CS low and check SDI level after sending a command. The question is :

  - Can I read the SDI signal as a standard GPIO ?

Thank you for supporting 

Franck

0 Kudos
Reply
1 Solution
883 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Franck,

yes, you can, this is mentioned in the reference manual in section 12.6.1 Pin control:

lukaszadrapa_0-1604510188172.png

Regards,

Lukas

 

View solution in original post

0 Kudos
Reply
2 Replies
872 Views
Franky31
Contributor I

Thank you Lukas !

Perfectly spot on. My bad I missed that point.

Regards

Franck

0 Kudos
Reply
884 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Franck,

yes, you can, this is mentioned in the reference manual in section 12.6.1 Pin control:

lukaszadrapa_0-1604510188172.png

Regards,

Lukas

 

0 Kudos
Reply