Hello,
I am using S32K144 EVB. It said "PEmicro GDB Launch Failure " after I have downlaod sevral times program to S32K144 by OpenSDA on the EVB. It show like this.
And I try to resove the problem:
1, Try different debug tool. I have try using PE multilink universal FX, and the result is same;
2, I press the reset button "SW1", the OpenSDA can go to bootloader mode, but the S32K144 is still working and can't be reset by the reset button "SW1".
3, I try to use full chip erase but the result is same. The config is show below
Is the GBD have some problem? I hope someone can help me, thank you!
Hi,
This issues doesn't look like an common problem.
Please check this post: Bricking and Recovering FRDM-KL25Z Boards: Reset, SWD Clock and Low Power | MCU on Eclipse and try P&E recovery utility chapter.
Best regards,
Razvan
I study the problem. I found the application program have been add new feature: PTA4 / JTAG_TMS,PTA5 / RESET, PTC4/ JTAG_TCK, PTC5/JTAG_TDI are be configged to GPIO. So after the EVB power on, the App is running, and the debug port are changed to GPIO, then OpenSDA conn't connect to the MCU.
So I replaced the EVB MCU with new one and it is working normal now!
I think there is maybe have another solution, but I don't know how to download a right App to MCU when the debug port is missing. If any body get it, please share me, thanks!