S32K144 Departition for Csec

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K144 Departition for Csec

Jump to solution
792 Views
XueZheng
Contributor I

Hello,

I have encountered problems during trying to enable the Csec feature on S32K144, and to do so, the first step I tried is to partition the flexNVM to 32K/32K and I found out that when the FCCOB1 is set to non-zero while the rest of FCCOB is set to exact same as Figure 5 in AN11983, then the operation is failed with FSTAT->ACCERR set.

XueZheng_0-1668499999516.png

For your information,

  1. This departition command is executed from RAM
  2. The Interrupt is suspended before executing this command
  3. Erase all blocks command and Program the secure field (0x40C) have been executed successfully before this command
  4. When the FCCOB1 is set to zero, the rest code is unchanged, then this command will be successful

 

0 Kudos
1 Solution
772 Views
XueZheng
Contributor I

@lukaszadrapa  thank you, after checking, the order information of MCU I used is S32K144HFVLH and the 'F' indicates "CANFD FlexIO" without security. I guess the higher version MCU of the S32K144 needs to be used to enable the Csec

View solution in original post

0 Kudos
2 Replies
777 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

this is working on my side. Which part number do you have exactly? Could you confirm it is device with CSEc?

lukaszadrapa_0-1668597685558.png

 

or if you have older device:

lukaszadrapa_1-1668597702090.png

Regards,

Lukas

0 Kudos
773 Views
XueZheng
Contributor I

@lukaszadrapa  thank you, after checking, the order information of MCU I used is S32K144HFVLH and the 'F' indicates "CANFD FlexIO" without security. I guess the higher version MCU of the S32K144 needs to be used to enable the Csec

0 Kudos