S32K142 boot to app ,diagnosis does not response.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K142 boot to app ,diagnosis does not response.

Jump to solution
2,154 Views
Ada_Lovelace
Contributor IV

Hi,all

I meet a problem, I set the project S32K142 from BOOT TO APP, app address:0x0010000,boot:0x0000,

I see the App sends the can message, I think it works,but when I download the app again, I find the APP does not response the diagnosis message.

I debug the App project individually,it can response diagnosis message and communication message.

But It has the problem when I download the app through the bootloader,App sends communication message,but it can not respond the diagnosis message.

What should I check to solve the problem?


Snipaste_2021-08-12_14-38-11.png

11 01 reset the project ,then jump to app , but it has no responds.

Snipaste_2021-08-12_14-44-21.png

 

0 Kudos
1 Solution
2,084 Views
Ada_Lovelace
Contributor IV

Hi,Jim

问题已经解决,can的初始化重新配置,buffer重新配置后,可以收到,可能是buffer一直被通信报文tx占用,rx buffer无法使用导致。

View solution in original post

0 Kudos
9 Replies
1,923 Views
Ada_Lovelace
Contributor IV

您好,

问题已经解决,应该与can配置有关。

0 Kudos
2,085 Views
Ada_Lovelace
Contributor IV

Hi,Jim

问题已经解决,can的初始化重新配置,buffer重新配置后,可以收到,可能是buffer一直被通信报文tx占用,rx buffer无法使用导致。

0 Kudos
2,080 Views
Senlent
NXP TechSupport
NXP TechSupport

好的收到,这个也是一个问题, 之前没遇到过,我这里会记录下来,写在以后的note里面。

0 Kudos
2,132 Views
Senlent
NXP TechSupport
NXP TechSupport

是不是中断向量表位置放错了,你试下呢,有进展给我回复一下,这个是我之前BOOT代码

Senlent_0-1628758916736.png

 

0 Kudos
2,108 Views
Ada_Lovelace
Contributor IV

Hi,Jim

尝试修改了,但是仍然不行。现象依旧。

 

Ada_Lovelace_0-1628761160948.png

Ada_Lovelace_1-1628761189612.png

 

0 Kudos
2,119 Views
Ada_Lovelace
Contributor IV

Hi,Jim

这个是我配置的,ld文件修改的内容,稍后试一下你说的内容,这个0x10400是vector的起始位置吗?

Ada_Lovelace_0-1628759931395.png

Ada_Lovelace_1-1628759978430.png

 

0 Kudos
2,144 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Ada_Lovelace

             11服务没用响应是允许的,这个是没有问题的。你自己想想,如果我没复位成功,我还可以给你发个否定响应,如果成功,ECU复位了,如何给你响应呢?每个服务它肯定是在成功执行服务请求后再发响应码,11服务特殊,它复位了,不发肯定响应码是对的。ISO14229中还有几个功能寻址的服务也没有响应码,详细的你可以看看ISO14229.(具体在什么地方我记不得,但是对于11服务没用肯定响应码这个我记忆犹新,而且我的上一个项目我也测试过,11服务成功是没用响应的。)

祝好!

 Jim.

0 Kudos
2,138 Views
Ada_Lovelace
Contributor IV

Hi,Jim.

问题不在于11的响应,而是第一次刷写后,已经跳转到APP了,可是这时候APP可以发出通信周期报文,可是诊断没有回复响应。而且这种情况只存在于boot跳转到APP的情况,现在通过boot烧录的app无法进行刷写流程。

如果我单独调试APP工程,我诊断是有响应的,我怀疑跳转的时候,出现了某些问题,请看看我跳转方式或者跳转前后需要调整哪些内容,来避免这个问题。

0 Kudos
2,134 Views
Senlent
NXP TechSupport
NXP TechSupport

这个不应该哎,APP按你的描述,APP还是可以正常工作,只是诊断没响应,这个怎么也说不过去阿。跳转到APP,除了诊断异常,其它工作正常嘛?,跳到APP的时候时钟从新更新下呢,APP和BOOT关于CAN的设置配置成一样试试。我花点时间看看我之前的工程,我给你找点我自前的配置。

0 Kudos