S32K142低温环境静态电流异常

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K142低温环境静态电流异常

1,146 Views
huangmingsong
Contributor III

产品在生产时,做高低温测试时,发现有部分不良产品低温情况下,静态功耗比正常的高出许多。如下图测试数据。S32K142芯片更换后产品静态电流正常了。芯片手册给出了25度以上的静态电流,25度以下的静态电流是否有管控标准或要求,目前测试来看,环境温度越低,差异越大。

image001(01-31-20-57-36).jpg

0 Kudos
Reply
3 Replies

1,113 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi mingsong,

1. 请问这个表格里的数据是S32K142芯片的电流,还是整个板子的电流?

2. 你提到的静态电流是指VLPS模式下的S32K142芯片电流吗?

3. 数据手册的“Table 13. Power consumption (Typicals unless stated otherwise)”表格里25℃、外设关闭情况下典型电流是29μA。但你的表格里在138μA左右,所以还开启了哪些外设吗?

4. 请查看数据手册的“Table 14. VLPS additional use-case power consumption at typical conditions”表格,检查有哪些增项:比如开启了哪些时钟或者外设。

5. VLPS模式下IO引脚电平会保持,请检查是否引脚连接的外部负载引起的。

6. 是否检查过S32K142的VDD电压有没变化?

7. 使用S32K142EVB测试SDK例程是否也会有同样的情况?芯片表面刻的mask号是多少?(不过0N33V的errata里看着也没相关的bug)

Best Regards,
Robin

0 Kudos
Reply

756 Views
huangmingsong
Contributor III

@Robin_Shen 

     是否有测试过低温情况下的功耗呢?目前客户这边由出现低功耗增大情况。

0 Kudos
Reply

1,111 Views
huangmingsong
Contributor III

这个电流是整板电流,MCU运行在VLPS模式下,同样的程序代码,呈现出低温情况下静态电流不一样 。

官方是否有低温下的静态电流测试情况?芯片出厂是否会测试低温情况的静态电流呢?

0 Kudos
Reply