Is anyone can help to check attached two projects?
They are almost the same, but the i2c output are different.
flexio_i2c_s32k118.7z works correctly. It will output "0x42, 0x51, 0x52, 0x53" every 3 seconds.
I export it's components and import to C120_TXBoard_20190805 project, and copy all .c .h files as well.
However, the output is "0x42, 0x43"....
flexio_i2c_s32k118 use linked resources for SDK or Project setting, I'm not sure if this causes the issue. I would like to use linked resources for C120_TXBoard_20190805 project, but I don't know how to do the change.
Hello Jimmy,
Sorry for the late response. I imported your project C120_TXBoard to my workspace and when I compiled it I received the following warnings.
These warnings are because you didn't add the following includes in your main.c file.
Could you please add this into your project to see if this solves the behavior you are facing?
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------