S32K118的pflash和dflash如何使用

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K118的pflash和dflash如何使用

跳至解决方案
241 次查看
Vapaus
Contributor III

S32K118的pflash和dflash如何配置并且使用

0 项奖励
回复
1 解答
214 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vapaus

You can find some flash examples inside the Real-Time Drivers (RTD) package.

Julin_AragnM_0-1717533601671.png

To install this RTD version you need to download the UpdateSite.zip file from the flexera portal. Once you have it, at S32DS Extensions and Updates, click "Add Update Site" and select the zip file, then click Open, you need to select the file and then Install.

Best regards,
Julián

在原帖中查看解决方案

0 项奖励
回复
1 回复
215 次查看
Julián_AragónM
NXP TechSupport
NXP TechSupport

Hi @Vapaus

You can find some flash examples inside the Real-Time Drivers (RTD) package.

Julin_AragnM_0-1717533601671.png

To install this RTD version you need to download the UpdateSite.zip file from the flexera portal. Once you have it, at S32DS Extensions and Updates, click "Add Update Site" and select the zip file, then click Open, you need to select the file and then Install.

Best regards,
Julián

0 项奖励
回复