S32K1 DUAL BANK OTA___AB SWAP OTA DEMO

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K1 DUAL BANK OTA___AB SWAP OTA DEMO

Jump to solution
1,059 Views
sophie-wang
Contributor III

Dear NXP Friend,

Does NXP have dual bank ota demo or ab swap ota demo for S32K1?

Thank you

Sophie

0 Kudos
Reply
1 Solution
1,033 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @sophie-wang 

We provide application note “S32K1xx Firmware updates” discussing A/B swap and using CAN interface:

https://www.nxp.com/docs/en/application-note/AN12323.pdf

https://www.nxp.com/docs/en/application-note-software/AN12323SW.zip

There are SW examples for S32K144 and S32K146.

S32K144 has one read partition on program flash, so it is not possible to update the application while the old application is still running.

S32K146 has more read partitions on program flash, so old application can run during the update.

Regards,

Lukas

View solution in original post

1 Reply
1,034 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi @sophie-wang 

We provide application note “S32K1xx Firmware updates” discussing A/B swap and using CAN interface:

https://www.nxp.com/docs/en/application-note/AN12323.pdf

https://www.nxp.com/docs/en/application-note-software/AN12323SW.zip

There are SW examples for S32K144 and S32K146.

S32K144 has one read partition on program flash, so it is not possible to update the application while the old application is still running.

S32K146 has more read partitions on program flash, so old application can run during the update.

Regards,

Lukas