S32K ADC,What is Source impedance(Rs) when fadck=40MHz

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32K ADC,What is Source impedance(Rs) when fadck=40MHz

跳至解决方案
534 次查看
Muskz
Contributor II

About S32K ADC,Frome datasheet for S32K devices, ,we know Source impedance(Rs)  max is 5K,conditions is fadck < 4MHz.

Can I understand it this way? If I use an adc clock that is less than 4M, the maximum allowable Rs for external circuits is 5k.
If I use an adc clock of 40M, what should be the Rs? Why is it not stated in the manual, should it be larger or smaller than 5k?

I have read the manual AN12217, S32K1xx ADC guidelines, spec and configuration, but I haven't found any useful answers. Perhaps my level is not high enough

 

Thank you.

 

0 项奖励
回复
1 解答
500 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Muskz,

Sorry. DataSheet does not give the source impedance (Rs) at fadck=40MHz.

Please read the AN4373 Cookbook for SAR ADC Measurements mentioned in AN12217. I think it should be smaller than 5k.

AN12217 AN4373.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

2 回复数
485 次查看
Muskz
Contributor II

Thank you very much for the information you provided. I will read the relevant documents.

0 项奖励
回复
501 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi Muskz,

Sorry. DataSheet does not give the source impedance (Rs) at fadck=40MHz.

Please read the AN4373 Cookbook for SAR ADC Measurements mentioned in AN12217. I think it should be smaller than 5k.

AN12217 AN4373.jpg


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------