I wondered that
if erased CAN Source, Errors not occured.
but if add CAN Source, paralyzed all CAN_Node associated to CAN_BUS.
If our CAN node can influenced on CAN_BUS without TX ??
(our CAN source code has only RX)
On the other side, ARM CAN source doesn't occur error.
Hi,
would be great to know how such paralyze looks like. Ideally check for errors detected on nodes and measure your node TXD/RXD and CAN signals.
Even if node is not transmitting a message it receives frames and ACKs it back and in case of any error detected it sends error frame.
If you need not TX on node you can try to use LOM (Listen Only Mode).
BR, Petr
Are you saying that I can receive it as an RX signal and reply the error frame without sending the TX signal from NODE?
and Does the error frame sent over the ACK signal also cause errors on other nodes of CAN_BUS?