S32K 144 Unified bootloader could not work well

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32K 144 Unified bootloader could not work well

1,632 Views
KILLERzheng
Contributor IV

Hi, NXP

I download the unified bootloader setup file and extract the archive.

In this archive, I import the S32K144_UDS_Bootloader_App_Test project. It could build pass, however it could not work when I debug with PE, and it goes wrong at the first step initClock().

I do not know where the fault is, could you please help me?

 

KILLERzheng_0-1642664949411.png

KILLERzheng_1-1642665138669.png

 

0 Kudos
10 Replies

1,621 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@KILLERzheng

the .ld file is already modified,that's why you can not debug it.

Senlent_0-1642670062891.png

 

0 Kudos

1,614 Views
KILLERzheng
Contributor IV

Hi Senlent,

I think I  have not modified any file,  and how to deal with it?

0 Kudos

1,602 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@KILLERzheng

please compare with other different project regarding the .ld file, then  you may see the difference.

0 Kudos

1,598 Views
KILLERzheng
Contributor IV

I modified the .ld file(compare with the S32K144_CAN_bootloader project in this archive), and reference to the UBLUG, but it still could not work well

 

KILLERzheng_0-1642675996849.png

KILLERzheng_1-1642676137036.png

KILLERzheng_2-1642676162566.png

 

 

0 Kudos

1,584 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@KILLERzheng

/*
** ###################################################################
**     Processor:           S32K144 with 64 KB SRAM
**     Compiler:            GNU C Compiler
**
**     Abstract:
**         Linker file for the GNU C Compiler
**
**     Copyright (c) 2015-2016 Freescale Semiconductor, Inc.
**     Copyright 2017-2018 NXP
**     All rights reserved.
**
**     THIS SOFTWARE IS PROVIDED BY NXP "AS IS" AND ANY EXPRESSED OR
**     IMPLIED WARRANTIES, INCLUDING, BUT NOT LIMITED TO, THE IMPLIED WARRANTIES
**     OF MERCHANTABILITY AND FITNESS FOR A PARTICULAR PURPOSE ARE DISCLAIMED.
**     IN NO EVENT SHALL NXP OR ITS CONTRIBUTORS BE LIABLE FOR ANY DIRECT,
**     INDIRECT, INCIDENTAL, SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES
**     (INCLUDING, BUT NOT LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR
**     SERVICES; LOSS OF USE, DATA, OR PROFITS; OR BUSINESS INTERRUPTION)
**     HOWEVER CAUSED AND ON ANY THEORY OF LIABILITY, WHETHER IN CONTRACT,
**     STRICT LIABILITY, OR TORT (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING
**     IN ANY WAY OUT OF THE USE OF THIS SOFTWARE, EVEN IF ADVISED OF
**     THE POSSIBILITY OF SUCH DAMAGE.
**
**     http:                 www.freescale.com
**     mail:                 support@freescale.com
**
** ###################################################################
*/

/* Entry Point */
ENTRY(Reset_Handler)

HEAP_SIZE  = DEFINED(__heap_size__)  ? __heap_size__  : 0x00000400;
STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x00000400;

/* If symbol __flash_vector_table__=1 is defined at link time
 * the interrupt vector will not be copied to RAM.
 * Warning: Using the interrupt vector from Flash will not allow
 * INT_SYS_InstallHandler because the section is Read Only.
 */
M_VECTOR_RAM_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : 0x0400;

/* Specify the memory areas */
MEMORY
{
  /* Flash */
  m_interrupts          (RX)  : ORIGIN = 0x00000000, LENGTH = 0x00000400
  m_flash_config        (RX)  : ORIGIN = 0x00000400, LENGTH = 0x00000010
  m_text                (RX)  : ORIGIN = 0x00000410, LENGTH = 0x0007FBF0

  /* SRAM_L */
  m_data                (RW)  : ORIGIN = 0x1FFF8000, LENGTH = 0x00008000

  /* SRAM_U */
  m_data_2              (RW)  : ORIGIN = 0x20000000, LENGTH = 0x00007000
}

/* Define output sections */
SECTIONS
{
  /* The startup code goes first into internal flash */
  .interrupts :
  {
    __VECTOR_TABLE = .;
    __interrupts_start__ = .;
    . = ALIGN(4);
    KEEP(*(.isr_vector))     /* Startup code */
    __interrupts_end__ = .;
    . = ALIGN(4);
  } > m_interrupts

  .flash_config :
  {
    . = ALIGN(4);
    KEEP(*(.FlashConfig))    /* Flash Configuration Field (FCF) */
    . = ALIGN(4);
  } > m_flash_config

  /* The program code and other data goes into internal flash */
  .text :
  {
    . = ALIGN(4);
    *(.text)                 /* .text sections (code) */
    *(.text*)                /* .text* sections (code) */
    *(.rodata)               /* .rodata sections (constants, strings, etc.) */
    *(.rodata*)              /* .rodata* sections (constants, strings, etc.) */
    *(.init)                 /* section used in crti.o files */
    *(.fini)                 /* section used in crti.o files */
    *(.eh_frame)             /* section used in crtbegin.o files */
    . = ALIGN(4);
  } > m_text

  /* Section used by the libgcc.a library for fvp4 */
  .ARM :
  {
    __exidx_start = .;
    *(.ARM.exidx*)
    __exidx_end = .;
  } > m_text

  __etext = .;    /* Define a global symbol at end of code. */
  __DATA_ROM = .; /* Symbol is used by startup for data initialization. */

  .interrupts_ram :
  {
    . = ALIGN(4);
    __VECTOR_RAM__ = .;
    __RAM_START = .;
    __interrupts_ram_start__ = .; /* Create a global symbol at data start. */
    *(.m_interrupts_ram)          /* This is a user defined section. */
    . += M_VECTOR_RAM_SIZE;
    . = ALIGN(4);
    __interrupts_ram_end__ = .;   /* Define a global symbol at data end. */
  } > m_data

  __VECTOR_RAM = DEFINED(__flash_vector_table__) ? ORIGIN(m_interrupts) : __VECTOR_RAM__ ;
  __RAM_VECTOR_TABLE_SIZE = DEFINED(__flash_vector_table__) ? 0x0 : (__interrupts_ram_end__ - __interrupts_ram_start__) ;

  .data : AT(__DATA_ROM)
  {
    . = ALIGN(4);
    __DATA_RAM = .;
    __data_start__ = .;      /* Create a global symbol at data start. */
    *(.data)                 /* .data sections */
    *(.data*)                /* .data* sections */
    . = ALIGN(4);
    __data_end__ = .;        /* Define a global symbol at data end. */
  } > m_data

  __DATA_END = __DATA_ROM + (__data_end__ - __data_start__);
  __CODE_ROM = __DATA_END; /* Symbol is used by code initialization. */

  .code : AT(__CODE_ROM)
  {
    . = ALIGN(4);
    __CODE_RAM = .;
    __code_start__ = .;      /* Create a global symbol at code start. */
    __code_ram_start__ = .;
    *(.code_ram)             /* Custom section for storing code in RAM */
    . = ALIGN(4);
    __code_end__ = .;        /* Define a global symbol at code end. */
    __code_ram_end__ = .;
  } > m_data

  __CODE_END = __CODE_ROM + (__code_end__ - __code_start__);
  __CUSTOM_ROM = __CODE_END;

  /* Custom Section Block that can be used to place data at absolute address. */
  /* Use __attribute__((section (".customSection"))) to place data here. */
  .customSectionBlock  ORIGIN(m_data_2) : AT(__CUSTOM_ROM)
  {
    __customSection_start__ = .;
    KEEP(*(.customSection))  /* Keep section even if not referenced. */
    __customSection_end__ = .;
  } > m_data_2
  __CUSTOM_END = __CUSTOM_ROM + (__customSection_end__ - __customSection_start__);

  /* Uninitialized data section. */
  .bss :
  {
    /* This is used by the startup in order to initialize the .bss section. */
    . = ALIGN(4);
    __BSS_START = .;
    __bss_start__ = .;
    *(.bss)
    *(.bss*)
    *(COMMON)
    . = ALIGN(4);
    __bss_end__ = .;
    __BSS_END = .;
  } > m_data_2

   /* Put heap section after the program data */
  .heap :
  {
    . = ALIGN(8);
    __end__ = .;
    __heap_start__ = .;
    PROVIDE(end = .);
    PROVIDE(_end = .);
    PROVIDE(__end = .);
    __HeapBase = .;
    . += HEAP_SIZE;
    __HeapLimit = .;
    __heap_limit = .;
    __heap_end__ = .;
  } > m_data_2

  /* Initializes stack on the end of block */
  __StackTop   = ORIGIN(m_data_2) + LENGTH(m_data_2);
  __StackLimit = __StackTop - STACK_SIZE;
  PROVIDE(__stack = __StackTop);
  __RAM_END = __StackTop;

  .stack __StackLimit :
  {
    . = ALIGN(8);
    __stack_start__ = .;
    . += STACK_SIZE;
    __stack_end__ = .;
  } > m_data_2

  .ARM.attributes 0 : { *(.ARM.attributes) }

  ASSERT(__StackLimit >= __HeapLimit, "region m_data_2 overflowed with stack and heap")
}

0 Kudos

1,537 Views
KILLERzheng
Contributor IV

I find that the PLL configuration is wrong, when I set the PLL false, then it could init success and could transmit can message(500k).

But I still don't know why the PLL configuration is wrong, and how to config it

0 Kudos

1,519 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@KILLERzheng

    Did you test it after replacing the .id files as I said before?

     I have tested the project and everything is ok.

Senlent_0-1643077456209.png

 

 

0 Kudos

1,490 Views
KILLERzheng
Contributor IV

I import the code into the project, but it still could not work. Here the projects are, and both of them could not debug. I have no idea how to deal with it, could you please help me?

0 Kudos

1,514 Views
KILLERzheng
Contributor IV

I did replace the *.ld file and test the newer project, but it still could not work as usual.

However, when I set the PLL false while I use the default *.ld file, it could work.

Is the PLL configuration conflicted with the *.ld file configuration??

0 Kudos

1,579 Views
KILLERzheng
Contributor IV

Hi Senlent,

I import the code into the project, but it still could not work. Here the projects are, and both of them could not debug. I have no idea how to deal with it, could you please help me?

0 Kudos