S32DS3.4 add the FlexCan RTD Driver in S32K312 project issue

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS3.4 add the FlexCan RTD Driver in S32K312 project issue

ソリューションへジャンプ
1,516件の閲覧回数
Bert2023
Contributor I

Hi Sir:

IThe chip we use is S32K312,add the FlexCan RTD Driver ,it did not  build success. More inform as below:

Tool:S3DS3.4

RTD:PlatformSDK_S32K3_2022_07   version:2.0.1

the error information as attachment picture error.jpg。

Thanks!

0 件の賞賛
返信
1 解決策
1,462件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Bert2023

you may forgot to update code here.

Senlent_0-1684736524033.png

 

元の投稿で解決策を見る

0 件の賞賛
返信
5 返答(返信)
1,465件の閲覧回数
Bert2023
Contributor I

Hi,Senlent:

Thanks for you reply.

I use the  demo "FlexCAN_Ip_Example_S32K312" provided in RTD or New creat a project  and remove the “compatibility.xml” file the error information (Newcreat.jpg),the demo error inforation (FlexCAN_Ip_Example_S32K312.jpg) as attachment picture.

0 件の賞賛
返信
1,463件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Bert2023

you may forgot to update code here.

Senlent_0-1684736524033.png

 

0 件の賞賛
返信
1,385件の閲覧回数
Bert2023
Contributor I
Hi Senlent:
It‘s ok after update code。
Thanks!
0 件の賞賛
返信
1,480件の閲覧回数
Senlent
NXP TechSupport
NXP TechSupport

Hi@Bert2023

Can you try to test the demo "FlexCAN_Ip_Example_S32K312" provided in RTD?

If this problem still exists,this may be a known bug of S32 DS V3.4 ,please try to remove the “compatibility.xml” located at “C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration.

BR!

0 件の賞賛
返信
766件の閲覧回数
wang0063
Contributor I

Can  you  provide the demo of "FlexCAN_Ip_Example_S32K312"?

0 件の賞賛
返信