S32DS3.4 add the FlexCan RTD Driver in S32K312 project issue

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS3.4 add the FlexCan RTD Driver in S32K312 project issue

Jump to solution
1,519 Views
Bert2023
Contributor I

Hi Sir:

IThe chip we use is S32K312,add the FlexCan RTD Driver ,it did not  build success. More inform as below:

Tool:S3DS3.4

RTD:PlatformSDK_S32K3_2022_07   version:2.0.1

the error information as attachment picture error.jpg。

Thanks!

0 Kudos
Reply
1 Solution
1,465 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Bert2023

you may forgot to update code here.

Senlent_0-1684736524033.png

 

View solution in original post

0 Kudos
Reply
5 Replies
1,468 Views
Bert2023
Contributor I

Hi,Senlent:

Thanks for you reply.

I use the  demo "FlexCAN_Ip_Example_S32K312" provided in RTD or New creat a project  and remove the “compatibility.xml” file the error information (Newcreat.jpg),the demo error inforation (FlexCAN_Ip_Example_S32K312.jpg) as attachment picture.

0 Kudos
Reply
1,466 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Bert2023

you may forgot to update code here.

Senlent_0-1684736524033.png

 

0 Kudos
Reply
1,388 Views
Bert2023
Contributor I
Hi Senlent:
It‘s ok after update code。
Thanks!
0 Kudos
Reply
1,483 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Bert2023

Can you try to test the demo "FlexCAN_Ip_Example_S32K312" provided in RTD?

If this problem still exists,this may be a known bug of S32 DS V3.4 ,please try to remove the “compatibility.xml” located at “C:\NXP\S32DS.3.4\eclipse\mcu_data\configuration.

BR!

0 Kudos
Reply
769 Views
wang0063
Contributor I

Can  you  provide the demo of "FlexCAN_Ip_Example_S32K312"?

0 Kudos
Reply