S32DS creates S32K341 and S32K342 without J-LINK debugging options

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32DS creates S32K341 and S32K342 without J-LINK debugging options

Jump to solution
349 Views
jiafeimao
Contributor III

When I use S32DS to create the S32K344 project, I can choose GDB PEMicro and Segger in the debug options. However, when I create the S32K342/S32K341 project, only GDB PEMicro is available without the Segger option. How can I use J-LINK to debug my S32K341 project?

jiafeimao_0-1714017289560.png

 

0 Kudos
Reply
1 Solution
328 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@jiafeimao

I forgot that J-LINK does not support S32K341&S32K342

Then it cannot be supported, because essentially S32 DS is implemented by calling J-link DLL.

View solution in original post

0 Kudos
Reply
3 Replies
331 Views
jiafeimao
Contributor III

Thank you for providing the information. S32K341 is not on SEGGER's support list. Are you aware of this? The following image shows the S32K3 series supported by SEGGER's J-LINK, which includes S32K342 and S32K344. Unfortunately, S32K341 is not included. We look forward to any suggestions from you.

jiafeimao_0-1714023395695.png

 

0 Kudos
Reply
329 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@jiafeimao

I forgot that J-LINK does not support S32K341&S32K342

Then it cannot be supported, because essentially S32 DS is implemented by calling J-link DLL.

0 Kudos
Reply
335 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
Reply