S32DS can't install freertos for S32K344

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32DS can't install freertos for S32K344

跳至解决方案
85 次查看
Hanoch
Contributor II

Hi everyone,

What I saw a post just now is the same as my subject. when I install the offline installation package, I also found I can't install freertos, reporting one or more required tiems could not be found. image as follows:

Hanoch_0-1715258273379.png

it show that I had installed the software., nstallation details as follows: 

Hanoch_2-1715258347550.png

but I can't create new freertos project from k3 example, images as follows:

Hanoch_3-1715258447401.png

how do I install successfully?

 

 

 

标记 (1)
0 项奖励
1 解答
64 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hanoch 

The FreeRTOS version 2.0.3 was developed for S32DS v3.4 using S32K3 Real-Time Drivers AUTOSAR 4.4 Version 2.0.3. According to the provided information, you are using S32DS v3.5 and RTD v3.0.0; the FreeRTOS version compatible with this SW is the 3.1.0 (SW32K3_FreeRTOS_10.5.1_3.1.0_D2304).

 

B.R.

VaneB

在原帖中查看解决方案

0 项奖励
2 回复数
65 次查看
VaneB
NXP TechSupport
NXP TechSupport

Hi @Hanoch 

The FreeRTOS version 2.0.3 was developed for S32DS v3.4 using S32K3 Real-Time Drivers AUTOSAR 4.4 Version 2.0.3. According to the provided information, you are using S32DS v3.5 and RTD v3.0.0; the FreeRTOS version compatible with this SW is the 3.1.0 (SW32K3_FreeRTOS_10.5.1_3.1.0_D2304).

 

B.R.

VaneB

0 项奖励
55 次查看
Hanoch
Contributor II

Thanks, it's done!

0 项奖励