S32DS 下 S32K144 如何添加和使用FFT变换

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

S32DS 下 S32K144 如何添加和使用FFT变换

1,731件の閲覧回数
gaowei
Contributor I

请教下,请问谁知到在S32DS如环境中如何使用 S32K144 的dsp功能来做FFT变换?急用,谢谢!

0 件の賞賛
返信
3 返答(返信)

1,623件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Wei,

I'm aware of two DSP libraries:

- CMSIS DSP which is not included in S32 Design Studio but you can download official release from ARM web site and use the library in your project:

https://developer.arm.com/tools-and-software/embedded/cmsis

- AMMCLIB which is included in S32 Design Studio. AMMCLIB has many DSP functions and should have better performance than CMSIS  DSP.

Regards,

Lukas

0 件の賞賛
返信

1,623件の閲覧回数
gaowei
Contributor I

Thank you for your help!

gaowei@auratec.com.cn

发件人: lukaszadrapa

发送时间: 2020-04-28 12:40

收件人: wei gaowei

主题: Re: - Re: S32DS 下 S32K144 如何添加和使用FFT变换

NXP Community

Re: S32DS 下 S32K144 如何添加和使用FFT变换

reply from Lukas Zadrapa in S32K - View the full discussion

Hi Wei,

I'm aware of two DSP libraries:

- CMSIS DSP which is not included in S32 Design Studio but you can download official release from ARM web site and use the library in your project:

https://developer.arm.com/tools-and-software/embedded/cmsis

- AMMCLIB which is included in S32 Design Studio. AMMCLIB has many DSP functions and should have better performance than CMSIS DSP.

Regards,

Lukas

Reply to this message by replying to this email, or go to the message on NXP Community

Start a new discussion in S32K by email or at NXP Community

Following Re: S32DS 下 S32K144 如何添加和使用FFT变换 in these streams: Inbox

This email was sent by NXP Community because you are a registered user.

You may unsubscribe instantly from NXP Community, or adjust email frequency in your email preferences

0 件の賞賛
返信

1,623件の閲覧回数
gaowei
Contributor I

S32K144 is a car standard MCU launched by NXP, the kernel is cortex-m4f, with FPU and DSP functions,However, it is rare to see the use of methods or routines, very hope that someone familiar with this kind of content to give answers

0 件の賞賛
返信