S32 Design stdudio -->Description No such file or directory

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S32 Design stdudio -->Description No such file or directory

Jump to solution
1,684 Views
Alanzero
Contributor I

For the S32K144  Development Board。

    I download  one project  by  S32 Design stdudio ,some error showed when build the project。
    Even if I add header files to the project, I still report an error

 

0 Kudos
1 Solution
1,494 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alanzero

change highlighted jumper to 2 & 3 and try again.

Senlent_0-1694507324888.png

All of your problems come from not reading the guide to becoming familiar with your development environment.

View solution in original post

0 Kudos
18 Replies
1,669 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alanzero

I can't help you without more info.

Can you provide more info about your problem, such as the version of IDE and SDK,also the project you downloaded and the build error log.

0 Kudos
1,630 Views
Alanzero
Contributor I

HI Senlent

 the version:S32 Design Studio for ARM Version 2.2

T he ifo of error;03.png

0 Kudos
1,683 Views
Alanzero
Contributor I

01.png02.png

0 Kudos
1,626 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Akanzero

Thank you.

I see that you have added the paths of these files.

Maybe you should first check whether these files are under your project folder.

0 Kudos
1,621 Views
Alanzero
Contributor I

HI Senlent

I initially thought the header file was missing, but it actually exists

AS the following figure

04.png

After this problem appeared, I found some solutions online. For example, adding header files has no effect05.png
So need your help for give some recommendations to closed the error。

Thanks

0 Kudos
1,616 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alanzero

I'd like to help you,Is it possible to provide a project so that I can reproduce the problem?

0 Kudos
1,614 Views
Alanzero
Contributor I

HI Senlent

Project compression package, as attached

Thanks

0 Kudos
1,598 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alanzero

I just imported the compressed package you provided, and there was no problem with compilation.

Senlent_0-1694488358607.png

 

0 Kudos
1,595 Views
Alanzero
Contributor I

HI Senlent
   Using the following import,which I need to choose in the  item?

Alanzero_0-1694488529859.png
 I used to use Open projects from file system

Alanzero_1-1694488755963.png

 

 

0 Kudos
1,591 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alanzero

 

Senlent_0-1694488980464.png

Senlent_1-1694488990648.png

 

0 Kudos
1,545 Views
Alanzero
Contributor I

HI  Senlent
 This project Compilation passed,but i can't find the download options 0.0

Alanzero_0-1694489359855.png

0 Kudos
1,539 Views
Senlent
NXP TechSupport
NXP TechSupport
0 Kudos
1,529 Views
Alanzero
Contributor I

HI Senlent
After build the project,This window pops up,I try some way to change the config,but never resolved

Alanzero_0-1694501599208.png

 

0 Kudos
1,525 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alanzero

Is this your first using S32 DS?

Can other projects be connected normally?

Can you refer to the debugging interface configuration of a normally working project?

0 Kudos
1,521 Views
Alanzero
Contributor I

HI  Senlent

 yes,It’s the frist time to use S32 DS,when I download the APP,the problem is bothering me until now。

So in use the APP,so much  questions perplex me。Luckly, this forum exists

 

0 Kudos
1,509 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alanzero

good news, if your problem are solved, you can click "ACCEPT AS SOLUTION" to close this topic.

0 Kudos
1,507 Views
Alanzero
Contributor I

HI   Senlent
This is the development board I am using. What should be its interface configuration to solve this problem

Alanzero_1-1694506348686.png

Alanzero_2-1694506504205.png

 

0 Kudos
1,495 Views
Senlent
NXP TechSupport
NXP TechSupport

Hi@Alanzero

change highlighted jumper to 2 & 3 and try again.

Senlent_0-1694507324888.png

All of your problems come from not reading the guide to becoming familiar with your development environment.

0 Kudos