S32 Configuration Tool Dio Channel ID error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

S32 Configuration Tool Dio Channel ID error

跳至解决方案
254 次查看
Vast-Horizon
Contributor I

Hello,

I'm new to MBDT and the S32 Configuration Tool. I want to make a simple blinking LED project using MBDT with S32K358. From the datasheet, I notice the following information:

Pin number: 86

Pin name: PTC21

Pin type: OUT

Purpose: LED_GRN

So I thought the Port ID was 5 for PTC [31-16]

VastHorizon_0-1714105479905.png

and the channel ID was 21. However, it looks like I misunderstood something because it said the channel id is out of range:

VastHorizon_1-1714105597260.png

VastHorizon_2-1714105752047.png

 

What should I do to properly configure this pin? Thanks.

 

 

0 项奖励
回复
1 解答
230 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The value of Dio Channel Id must be in range: 0-15
For PTC21 please enter 5 (21-16)

Please notice that Model Based Design Tools (MBDT) are supported by our engineers on this community:
https://community.nxp.com/community/mbdt
It’s an exception, all our products are supported via these tickets but except these MBDT tools. So, create please new thread on the community and responsible engineers will help you.
Thanks for understanding.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
2 回复数
70 次查看
Esakki
Contributor II

Hello nxp team,

we are trying to enable the PTD17 pin high with dio peripheral

port name: PTD_H

Dio port Id: 7

Dio channel Id: 1

how to check the channel id i set is correct or not?

right now this pin is not getting high

0 项奖励
回复
231 次查看
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

The value of Dio Channel Id must be in range: 0-15
For PTC21 please enter 5 (21-16)

Please notice that Model Based Design Tools (MBDT) are supported by our engineers on this community:
https://community.nxp.com/community/mbdt
It’s an exception, all our products are supported via these tickets but except these MBDT tools. So, create please new thread on the community and responsible engineers will help you.
Thanks for understanding.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复