S2K144 LPIT

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

S2K144 LPIT

735 Views
zq1
Contributor III

in the picture below,when the counter add 1,it means  1 us ?

after counter reach to 1000 000 ,it will generate intrupt ???

the peroiod of interrupt is 1 s  ???

it is  nothing without  the frequency of my  device ?

the trriger source must chose internal trriger if i want to use it as a 1s timer   ?????

zq1_0-1689147629368.png

hope your reply

0 Kudos
Reply
2 Replies

725 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Because you selected Microsecond unit in Period units, so when the counter add 1,it means  1 us(Microsecond).
Yes. After counter reach to 1000 000 ,it will generate interrupt. The period of interrupt is 1 s .

Q: It is  nothing without  the frequency of my  device?
A: Yes. Because you selected Microsecond unit in Period units. The driver will calculate it according to the frequency of your device. 

Q: the trigger source must chose internal trigger if I want to use it as a 1s timer   ?????
A: No. Please test lpit_periodic_interrupt_s32k144 in S32K1 SDK, the example is configured to trigger an interrupt every second, which toggles a LED.

Regarding the LPIT module, you can also refer to AN5413 S32K1xx Series Cookbook.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply

689 Views
zq1
Contributor III

thanks for your reply.

but i have test the question ,the frequency of clock is 16MHZ,when i set the counter periodic to 16000000,

when the counter reach to 16000000,it generates interrupt,inn the intrrupt hander function,i make the led reverse,the led is on with 2 second period, so i think ,the interrupt period is related to the LPIT0_CLK

0 Kudos
Reply