Request Manual of transceivers used in S32K3X4EVB-T172 Evaluation Board

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Request Manual of transceivers used in S32K3X4EVB-T172 Evaluation Board

ソリューションへジャンプ
1,141件の閲覧回数
mrtientv6
Contributor II

Dear Expert,

We bought S32K3X4EVB-T172 Evaluation Board for development. (S32K3X4EVB-T172 Evaluation Board for Automotive General Purpose | NXP Semiconductors)

But we cannot find manual, datasheet and example source code to control CAN, LIN and ETH transceivers. 

Could you help to provide to us these inputs?

 

Thanks.
Tien Tran

0 件の賞賛
返信
1 解決策
1,074件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) refer to https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS
2) for Eth PHY init please refer to lwip demo included within TCPIP stack; download it from https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D and install it on top of used RTD drivers. Refer to release note doc to know how to install stack

BR, Petr  

元の投稿で解決策を見る

0 件の賞賛
返信
6 返答(返信)
1,118件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信
1,113件の閲覧回数
mrtientv6
Contributor II

Dear @PetrS 

Thank you for your information.

But as I check:

  1. For documentation, I cannot find Datasheet and manual of CAN and ETH transceiver. How can I request these secure documents?
  2. For RTD package of S32 Design Studio source code: NXP only provide example for loopback mode, no example source code to control or setting transceiver of CAN or ETH. Could you provide to us example source code to init Eth?

Could you please help us to feedback about these cases?

Thanks,
Tien Tran

0 件の賞賛
返信
1,075件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

1) refer to https://www.nxp.com/support/support/secure-access-rights:SEC-ACCESS
2) for Eth PHY init please refer to lwip demo included within TCPIP stack; download it from https://www.nxp.com/webapp/swlicensing/sso/downloadSoftware.sp?catid=SW32K3-REFSW-D and install it on top of used RTD drivers. Refer to release note doc to know how to install stack

BR, Petr  

0 件の賞賛
返信
945件の閲覧回数
imlaam
Contributor II

Hello @PetrS, I have run your example (lwip demo included within TCPIP stack) to activate ETH transceiver (TJA1103). However, the link establishment event was not happened. 

imlaam_0-1693474977759.png

imlaam_1-1693474987576.png

 

 

890件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

check for which boards is the example written for and tested on. The T172 has different pinout then the "Q" board, so correct pin configuration should be done as per board schematic. what is your T172 board revision?
Then how do you have board connected with PC? what kind of media converter do you use?

BR, Petr

0 件の賞賛
返信
1,080件の閲覧回数
mrtientv6
Contributor II

Dear @PetrS  and NXP experts,

Could you support to reply this ticket.
We need to use Eth in our board. Please help to provide ETH transceiver and sample init code to start Eth transmission.

Thanks,

TienTran

0 件の賞賛
返信