RTD version update question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTD version update question

464 Views
focusdoit
Contributor III

Hi Nxp experts,

I have a project created on RTD SW32K3_S32M27x_RTD_R21-11_4.0.0 on EB tresos, now I want to switch to RTD SW32K3_S32M27x_RTD_R21-11_4.0.0_P19.

Can I just replace the old link file SW32K3_S32M27x_RTD_R21-11_4.0.0.link with the new link file SW32K3_S32M27x_RTD_R21-11_4.0.0_P19.link?

Thanks

0 Kudos
Reply
3 Replies

439 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @focusdoit 

During the installation of the .exe, you can select the EB Tresos installation directory or you can copy all "<mod>_TS_T40D34M40I0R0" directories and .JAR files to the "<Tresos Install Path>\plugins" directory.

 

B.R.

VaneB

0 Kudos
Reply

436 Views
focusdoit
Contributor III

I mean the modules configured on old RTD, such as, Adc.xdm, Dem.xdm, Dio.xdm, Spi.xdum .. etc, can switch these configurations  to the new RTD smoothly?

0 Kudos
Reply

401 Views
VaneB
NXP TechSupport
NXP TechSupport

Hi @focusdoit 

The project maintains the files from the previous version. I am afraid that it will be required to create a new project with the new RTD version. 

0 Kudos
Reply