RTD 4.0 with Design Studio 3.5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

RTD 4.0 with Design Studio 3.5

Jump to solution
2,892 Views
Samuel_DCosta
Contributor III

I am using S32 Design Studio 3.5 for S32K344
Samuel_DCosta_0-1713018891635.png

I have downloaded 'SW32K3_RTD_R21-11_4.0.0_P16' and installed it. I would like to use RTD 4.0.0 along with the design studio version I have.

That means when I make some configuration from the S32 Config Tool and click 'Update Code', the RTD code should be updated according to 'SW32K3_RTD_R21-11_4.0.0_P16'


Currently, in Extension and Updates, I can only see RTD version 3.0.0

Samuel_DCosta_1-1713019098104.png


How do I link S32 Design Studio to RTD version 4.0.0?

0 Kudos
Reply
1 Solution
2,768 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

S32K3 RTD 4.0.0 is compatible with S32K344.
Which S32 Configuration Tool did you choose? Pins tool or Clocks tool or Peripherals tool? The other tools should not support S32K344. 

S32 Configuration Tool.png

If it is not the above problem, maybe some dependent software packages are missing during installation. It is recommended to refer to this post for offline installation: HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5

The following are the differences between installing S32K3 RTD3.0.0 and RTD 4.0.0:

Unchecking Contact all update sites during install to find required software can complete offline installation faster. (When you confirm that you only need to install these selected software)

Step2. S32 Design Studio 3.5 Update 8 D2311: SW32_S32DS_3.5.8_D2311.zip

Step3. Download and Install S32 Design Studio 3.5.8 Development Package with support for S32K3xx devices(3.5.8_D2311): SW32K3_S32DS_3.5.8_D2311.zip

Step4. Download and install S32K396 RTD for development, please download and install S32 Design Studio 3.5.6 RTM with support fo...(3.5.6_D2309): SW32K39x_S32DS_3.5.6_D2309.zip

Step5. If you only need S32K3 but not S32M2, you do not need to install the fifth step.

Step6. Download and install S32K3_Real-Time Drivers AUTOSAR R21-11 Version 4.0.0 Patch 16: SW32K3_RTD_R21-11_4.0.0_P16_DS_updatesite_D2404.zip
Need to install S32 Design Studio S32K396 SDK.

View solution in original post

0 Kudos
Reply
8 Replies
2,832 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi

Window -> Preferences -> S32 Design Studio for S32 Platform -> S32DS Extensions and Updates -> Add -> Archive...

Window Preferences S32 Design Studio for S32 Platform S32DS Extensions and Updates.png

Then SW32K3_RTD_R21-11_4.0.0_P16 should appear in S32DS Extensions and Updates.


Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply
2,785 Views
Samuel_DCosta
Contributor III

I have done as you suggested it works. I installed the RTD 4.0.0 as well from the 'S32DS Extensions and Updates' but I see this issue now

Samuel_DCosta_0-1713536118743.png


Is it that RTD 4.0.0 is not compatible with S32K344?

0 Kudos
Reply
2,769 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

S32K3 RTD 4.0.0 is compatible with S32K344.
Which S32 Configuration Tool did you choose? Pins tool or Clocks tool or Peripherals tool? The other tools should not support S32K344. 

S32 Configuration Tool.png

If it is not the above problem, maybe some dependent software packages are missing during installation. It is recommended to refer to this post for offline installation: HOWTO: offline install S32K3 RTD 3.0.0 in S32DS v3.5

The following are the differences between installing S32K3 RTD3.0.0 and RTD 4.0.0:

Unchecking Contact all update sites during install to find required software can complete offline installation faster. (When you confirm that you only need to install these selected software)

Step2. S32 Design Studio 3.5 Update 8 D2311: SW32_S32DS_3.5.8_D2311.zip

Step3. Download and Install S32 Design Studio 3.5.8 Development Package with support for S32K3xx devices(3.5.8_D2311): SW32K3_S32DS_3.5.8_D2311.zip

Step4. Download and install S32K396 RTD for development, please download and install S32 Design Studio 3.5.6 RTM with support fo...(3.5.6_D2309): SW32K39x_S32DS_3.5.6_D2309.zip

Step5. If you only need S32K3 but not S32M2, you do not need to install the fifth step.

Step6. Download and install S32K3_Real-Time Drivers AUTOSAR R21-11 Version 4.0.0 Patch 16: SW32K3_RTD_R21-11_4.0.0_P16_DS_updatesite_D2404.zip
Need to install S32 Design Studio S32K396 SDK.

0 Kudos
Reply
2,527 Views
Gwihan
Contributor II

When I tried, the difference between RTD 3.0.0 and RTD 4.0.0 does not ends at there.

The "Functional Group" name (as in 'Pins' ConfigTools) must match with PORT configuration.

The name <Your Port Name>_BOARD_InitPeripherals let you set <Your Port Name> in Port Configuration.

CfgGrpNames.pngPORTCfg.png

There was few more wired and minor miss-read of configuration setups. But, they are easily detected so that the correction did not took long time.

 

My RTD 4.0.0 installation is little different from the above (because I used package manager).install result.png

0 Kudos
Reply
2,512 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Please click ASK A QUESTION in the community. https://community.nxp.com/t5/S32K/bd-p/S32K

0 Kudos
Reply
2,569 Views
Gwihan
Contributor II

Irreproducible; the below message shows what I got after following the instruction.

install result.png

That configuration of packages is erroneous.

configure result.png

0 Kudos
Reply
2,559 Views
Robin_Shen
NXP TechSupport
NXP TechSupport

Step2. S32 Design Studio 3.5 Update 8 D2311: SW32_S32DS_3.5.8_D2311.zip

I did not install Update 11, not sure if it was caused by this.

0 Kudos
Reply
2,869 Views
RalphLIU
Contributor II

in case you have offline download the RTD version, you can install it from Help->install new software

0 Kudos
Reply