RTC Interrupt not working after VLPS->RUN mode transition

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

RTC Interrupt not working after VLPS->RUN mode transition

3,876件の閲覧回数
董超
Contributor II

Hi, s32k transmit from RUN mode to VLPS mode normally, then RTC alarm interrupt request wakeup MCU from VLPS mode to RUN mode, but RTC alarm interrupt not working  after VLPS to RUN mode transition.please answer , thanks!

0 件の賞賛
返信
5 返答(返信)

3,854件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

Hi 董超,

Please try to write TAR clears the SR[TAF] Time Alarm Flag in alarmISR.

alarmISR.pngTAF Time Alarm Flag.pngTAR Time Alarm Register.png

Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信

3,840件の閲覧回数
董超
Contributor II

Hi Robin:

Thanks for your reply,I write TAR clears the SR[TAF] Time Alarm Flag in Interrupt service function, I used RTC alarm repetition function to periodically wake up MCU when MCU transmits RUN -> VLPS -> RUN, i want to know wether RTC alarm interrupt trigger AWIC which is used to wakeup MCU or trigger NVIC executes interrupt service function at the same time?Look forward to your reply !!!ScreenHunter_026.bmp

0 件の賞賛
返信

3,829件の閲覧回数
Robin_Shen
NXP TechSupport
NXP TechSupport

RTC alarm interrupt trigger AWIC , it will wakeup MCU. After MCU is wakeup, it will run into RTC alarm interrupt.

Maybe you can refer the Example S32K144 RTC VLPS

0 件の賞賛
返信

3,812件の閲覧回数
董超
Contributor II

Hi Robin:

The RTC alarm interrupt triggers AWIC wakeup MCU, then trigger NVIC to execute interrupt service function, at this time, MCU is in run mode, but RTC interrupt is always suspended, can you help me?

微信截图_20210401014824.png

0 件の賞賛
返信

3,824件の閲覧回数
董超
Contributor II

Hi Robin:

I will try again with the example you provided, thanks !

 

0 件の賞賛
返信