Problem with load the program s32k3

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with load the program s32k3

2,114 Views
Miki849
Contributor II

Hi everybody, 

Today, I found a problem with my evaluation board . when i try program it , the s32 Ds give me the next error:

Error in final launch sequence:

Failed to execute MI command:
-exec-run
Error message from debugger back end:
Error creating process C:\Users\mgarcia\workspaceS32DS.3.4\Siul2_Dio_ToggleLed_S32K344\Debug_FLASH\Siul2_Dio_ToggleLed_S32K344.elf, (error 193).
Failed to execute MI command:
-exec-run
Error message from debugger back end:
Error creating process C:\Users\mgarcia\workspaceS32DS.3.4\Siul2_Dio_ToggleLed_S32K344\Debug_FLASH\Siul2_Dio_ToggleLed_S32K344.elf, (error 193).
Error creating process C:\Users\mgarcia\workspaceS32DS.3.4\Siul2_Dio_ToggleLed_S32K344\Debug_FLASH\Siul2_Dio_ToggleLed_S32K344.elf, (error 193).

 

I use the multilink programmer : https://es.rs-online.com/web/p/depuradores-y-emuladores-en-circuito/2194676?cm_mmc=ES-PLA-DS3A-_-goo...

And i can use it in another board without problem, moreover the program that i try to load , i used before without problem. And i can use it in another board too. 

Thank you so much in advance.

Kind regards 

 

Miguel

Tags (3)
0 Kudos
Reply
2 Replies

2,102 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Miguel,

if the same project works on another board and if the same Multilink works with another board, it points at the MCU/board. From HW point of view - did you try to measure supply voltages? Is the configuration the same (like jumpers)? Was the board handled according to ESD rules? From SW point of view - do you remember what was the last operation? Was that anything special?

Regards,

Lukas

0 Kudos
Reply

2,096 Views
Miki849
Contributor II

Hi Luka , 

The software we think is not the problem because we did nothing before connect to JTAG. 

We check with a thermal camera and we detect that we have a small hot point in the microchip so we think that the micro have a short circuit

0 Kudos
Reply