Hello,
I was using a program with CAN 0 to transmit messages and it was working fine. however, when making the change from CAN 0 to CAN 1 it stopped working, no message is transmitted by CAN.
I made the following changes in Processor Expert to use CAN 1:
Remove the configuration of the CAN0 pins and configure the PTA12 and PTA13 pins.
change the device from CAN 0 to CAN 1.
What could be the problem? Some other configuration change is required.
Thanks in advance!
已解决! 转到解答。
Hi
CAN0_TX(PTE5) and CAN0_RX(PTE4) are connected to UJA1169TK(CAN System Basis Chip), but those pins of CAN1 are not connected. You can find the information in S32K144EVB Evaluation Board Schematics.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hi
CAN0_TX(PTE5) and CAN0_RX(PTE4) are connected to UJA1169TK(CAN System Basis Chip), but those pins of CAN1 are not connected. You can find the information in S32K144EVB Evaluation Board Schematics.
Best Regards,
Robin
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------